Solar

OVERVIEW

Linking power to renewable growth

To meet an ever-growing need for power, the world is increasingly turning to renewable and sustainably-sourced energy.

 

In response to this demand, Prysmian’s cables are helping businesses in the solar industry around the globe to convert these new opportunities into reality.

Shining bright in the solar energy market

Always aware of our responsibility to the planet, we're constantly driving innovation in our industry, aiming to help renewable industry partners deliver projects with benefits for the future of both our world and their businesses.

And so, reflecting this commitment to both innovation and sustainability, we offer a full range of quality solar and photovoltaic products, renowned in the field for their easy installation, reliability and longevity attributes and complying with all major international standards.

Our customers

Our technologies are hard at work across the renewables sector, supporting the operations of contractors, developers, grid operators, PV panel makers, PV power generation system integrators and even entire solar parks.

In recent years, Prysmian Group has supplied components and services to worldwide solar installations from residential installation to large scale utility projects. The total equipment supplied exceeds a generation capacity of 40 GW.

Linking solar energy to the world’s
power needs, one cable at a time

Prysmian Group’s solar PV cable portfolio is composed of three brands:

  • Prysmian PRYSOLAR – the newest global brand, designed to face the most unpredictable challenges and anticipate the future. It is compliant with international standards EN 50618/IEC 62930. Upgraded with enhanced water endurance.

 

  • TECSUN - the premium brand made in Germany with over 15 years of experience and more than 1,000,000 km sold. This cable outperforms the standards of PV cables, is suited for the roughest conditions and for direct burial.

 

  • SUNGEN – the regional brand for markets like North American with local standards such as UL/CSA The Group’s solar PV cables are designed for the interconnection of various elements in photovoltaic systems, including panel interconnection, between panels and combiner boxes or from combiner boxes to the inverter.

Prysmian also offers complete cables solutions to enable the production and supply of solar energy. In addition to solar PV cables, the Group’s cable portfolio includes low, medium and high voltage cables according to the most known standards of each region, as well as special cables for communication and control.

In addition to cables, Prysmian offers electrical asset management solutions with PRY-CAM, the revolutionary technology for on-line, accurate and reliable partial discharge measurements, diagnosis and defect localization.

FOCUS ON

Prysmian PRYSOLAR

Prysmian PRYSOLAR is the Group’s global solar PhotoVoltaic (PV) wire compliant with international standards EN 50618/IEC 62930 and upgraded with enhanced water endurance.

FOCUS ON

TECSUN

A complete range of flexible cables for photovoltaic applications, especially developed for the use on the DC side at high temperatures (+120 °C) and under all climatic conditions.

Solare e Fotovoltaico

Tutte le informazioni sulla nostra eccezionale gamma di cavi per pannelli fotovoltaici, sviluppati in conformità con le disposizioni in materia e le classificazioni locali.

I cavi TECSUN sono ideali per la distribuzione di energia fotovoltaica grazie alle loro caratteristiche adatte allo spostamento libero e all’installazione in sospensione, con un intervallo di temperature comprese tra -40 e +120 °C. Questi cavi sono anche resistenti all'ammoniaca. Disponibili con omologazioni TÜV, UL e VDE.

Il Gruppo Prysmian offre ai propri clienti una gamma completa di soluzioni in cavo su misura.

 
Il Gruppo Prysmian offre ai propri clienti una gamma completa di soluzioni in cavo per il collegamento degli impianti fotovoltaici alla rete elettrica.

Discover our Global Product Range

11 Jan 2024

Cable Solutions for the Solar PV Industry

Renewables - Solar Product range

11 Jan 2024

Cable Solutions for the Solar PV Industry